i.MX6ULL based system using the the PF3000 PMIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL based system using the the PF3000 PMIC

916 Views
yuji_matsunami
Contributor II

Hello

I have a question for i.MX6ULL + PF3000.

Do you have application note for i.MX6ULL + PF3000 like AN5161 ?
Is the POR reset circuit the same as the i.MX6 SX based system circuit?

Best Regards,

Yuji Matsunami

0 Kudos
Reply
1 Reply

877 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yuji Matsunami,

There is not an application note per se, but there is a Reference Design with the i.MX6UL and the PF3000 (which is very similar to the i.MX6ULL, as you can see on AN5350) albeit this Reference Design is not public, so I would need to ask you to please open a ticket requesting the Design Files for this Reference Design.

My apologies for the inconvenience. 

Regards,

0 Kudos
Reply