i.MX6ULL VDD_SOC_IN maximum current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL VDD_SOC_IN maximum current

Jump to solution
600 Views
m_c
Senior Contributor I

In the i.MX6ULL referende design, the maximum current of VDD_SOC_IN shows 900mA, but 500mA in data sheet. Which one should be used when design customer board?

pastedImage_1.png

pastedImage_2.png

Labels (1)
0 Kudos
Reply
1 Solution
514 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Use data from the recent Datasheet.

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
1 Reply
515 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Use data from the recent Datasheet.

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply