i.MX6ULL UART(RTS CTS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL UART(RTS CTS)

1,023 Views
ban45
Contributor III

Hi

I swapped only CTS and RTS using the CnfigTools for i.MX Version 9.0, but no error or warning. (TX, RX are unchanged)
Which register should be changed to switch the functions in use? Is it possible to replace CTS and RTS without changing TX and RX?

best regard

0 Kudos
2 Replies

1,017 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

 

>Is it possible to replace CTS and RTS without changing TX and RX?

 

sorry this is not possible. For details one can look at Figure 55-2. UART external signals

to module signals routing with respect to DCE/DTE mode

i.MX 6ULL Applications Processor Reference Manual

 

Best regards
igor

0 Kudos

1,014 Views
ban45
Contributor III

Hi

Both can be set with the tool.
Do the RTS and CTS listed in the tool mean DCE / DTE = 0?

best regard

0 Kudos