Hello,
For the first case the maximum length of the single SPI burst is defined by FIFO. When FIFO is
underflowed (empty) the SS is negated. ECSPIx_PERIODREG may be used to setup delays between
SPI transfers.
For the second - multiple words, as defined in the BURST LENGTH field of the ECSPI_CONREG register,
will be transferred with SS negation.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.