i.MX6ULL GPMI NAND Flash driver example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6ULL GPMI NAND Flash driver example

1,400 次查看
jlin
Contributor I

Hi,

Is there a i.MX6ULL GPMI NAND Flash driver example? I did not find that in the SDK, probably because the EVK have NAND Flash as optional only (not populated by default).

标记 (1)
0 项奖励
回复
1 回复

1,300 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

one can look at

How-To use NAND boot on i.MX6UL EVK board 

https://community.nxp.com/thread/517143 

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/gpmi at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复