Dear Support-Team,
We understand that the sequence of power supply is below.
I.MX6ULL data sheet (IMX6ULLCEC 4.2)
-Specification
Power ON
· VDD_SNVS_IN -> VDD_HIGH_IN -> VDD_SOC_IN -> NVCC - xxx
Power OFF
· VDD_SOC_IN -> VDD_HIGH_IN -> VDD_SNVS_IN
By the way, it seems that the sequence of the evaluation board does not conform to the above specifications, is it good?
-i.MX6ULL-EVK
Power ON
• VDD_SOC_IN -> NVCC_xxx
The 3.3 V system of NVCC is simultaneously with VDD_HIGH_IN, and VDD_SOC_IN is turned on after that.
Power OFF
· VDD_SOC_IN -> VDD_HIGH_IN
It is dropping at the same time by discharge.
Best Regards,
Hi Tomohisa
you are right, sequence of the evaluation board was validated by nxp
and also may be recommended for use.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------