i.MX6ULL EVK design questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL EVK design questions

Jump to solution
1,438 Views
m_c
Senior Contributor I

In the page 10 of SPF-29364_A1.pdf, There is an MOSFET Q707 and gate pin connected with signal named DISCHG_EN.

1. What is function of Q707?

2. Can customer remove Q707 on their board?

3. Any side effect if remove Q707?

4. What is function of signal DISCHG_EN?

pastedImage_1.png

Labels (1)
1 Solution
1,334 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The discharge may be useful, when system reset is implemented as full power off and

then - on (in order to decrease discharge time). 

Regards,

Yuri.

View solution in original post

2 Replies
1,335 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The discharge may be useful, when system reset is implemented as full power off and

then - on (in order to decrease discharge time). 

Regards,

Yuri.

1,334 Views
mrudangshelat1
Senior Contributor II

Hi M.C

Q707 and DISCHG_EN signal is used to discharge the SOC voltage when power is turned off.

You can remove it if you do not want to use it.

Mrudang