In the page 10 of SPF-29364_A1.pdf, There is an MOSFET Q707 and gate pin connected with signal named DISCHG_EN.
1. What is function of Q707?
2. Can customer remove Q707 on their board?
3. Any side effect if remove Q707?
4. What is function of signal DISCHG_EN?
解決済! 解決策の投稿を見る。
Hello,
The discharge may be useful, when system reset is implemented as full power off and
then - on (in order to decrease discharge time).
Regards,
Yuri.
Hello,
The discharge may be useful, when system reset is implemented as full power off and
then - on (in order to decrease discharge time).
Regards,
Yuri.
Hi M.C
Q707 and DISCHG_EN signal is used to discharge the SOC voltage when power is turned off.
You can remove it if you do not want to use it.
Mrudang