i.MX6ULL EVK - Toggle BT_nPWD (BT_PWD_L)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL EVK - Toggle BT_nPWD (BT_PWD_L)

Jump to solution
1,282 Views
daweichen
Contributor III

Hi NXP,

Per the i.MX6ULL EVK schematic, BT_nPWD is routed to a serial-in-and-parallel-out register.

I am using the default imx6ull-14x14-evk.dts for NXP's i.MX6ULL EVK board.

Is there a way for me to toggle the state of this signal (BT_nPwD) via a Linux's user-space command during run-time?

I guess the alternative is to re-purpose (rewire) the BT_DISABLE, which I don't need for my Bluetooth module.

Thanks!

Dawei

Labels (2)
0 Kudos
1 Solution
1,158 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

in general it is possible as for example below

SPI Example: olinuxino GPIO expander 

Best regards
igor

View solution in original post

7 Replies
1,158 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

BT_nPwD is controlled by 74LV595PW  U2101  serial-out shift register

and I am afraid it not can be used directly through linux user-space commands.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,158 Views
daweichen
Contributor III

Hi Igor,

Thank you for the clarification. 

Is there a way to toggle the state of the signal?  (understand it can't be changed via a user-space command.)

dawei

0 Kudos
1,158 Views
daweichen
Contributor III

It looks like it can be changed through the DTS file.

                gpio_spi: gpio_spi@0 {
                        compatible = "fairchild,74hc595";
                        gpio-controller;
                        #gpio-cells = <2>;
                        reg = <0>;
                        registers-number = <1>;
                        registers-default = /bits/ 8 <0x57>;
                        spi-max-frequency = <100000>;

0 Kudos
1,158 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

it is necessary to send to 74LV595 data sequence

for changing that signal. One can look at 74LV595 datasheet

for more details. One can find on web helpful tutorials for gpio expanders, like:

Interfacing an I2C GPIO expander (MCP23017) to the Raspberry Pi using C++ (i2cdev) · Hertaville.com 

Best regards
igor

0 Kudos
1,158 Views
daweichen
Contributor III

Hi Igor,

I would like to do something quick. 

Would I be able to export BT_DISABLE (SNVS_TAMPER1) to sysfs and toggle the state by using the echo command?

If so, would you be able to tell my the correspond GPIO number?

Example: 

echo 106 > /sys/class/gpio/export

echo out > /sys/class/gpio/gpio106/direction
echo 0 > /sys/class/gpio/gpio106/value

Thanks,

dawei

0 Kudos
1,159 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dawei

in general it is possible as for example below

SPI Example: olinuxino GPIO expander 

Best regards
igor

1,158 Views
daweichen
Contributor III

Thank you very much, Igor.

I was able to export the gpio508 to sysfs and toggle the discrete output (BT_nPWD) state. 

By doing an "ls -la" command in the /sys/class/gpio directory command, I was able to see the spi-gpio expander starts with gpio number 504.

0 Kudos