i.MX6ULL DRAM_VREF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL DRAM_VREF

609 Views
ban45
Contributor III

Hi

About the voltage divider resistance of DRAM_VREF.
 
MX 6ULL Applications Processors for Industrial Products, Rev. 1.2, 11/2017 stated that it was 1.5kΩ ± 0.1%.
 
Hardware Development Guide for the i.MX 6ULL Applications Processor, Rev. 0, 08/2016 stated that it was 1.54kΩ ± 0.5%.
①What is the difference in resistance?
What happens with different tolerances?
➂Is it okay to use 1.5kΩ ± 0.5%?
Please tell me about ① ~ ③.
 

best regard

0 Kudos
Reply
3 Replies

604 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Generally both variants (1.5kΩ ± 0.1% and 1.54kΩ ± 0.5%) are acceptable.
The variant 1.5kΩ ± 0.5% also is possible, but 0.1% resistors accuracy is more preferable.

 

Regards,
Yuri.

0 Kudos
Reply

596 Views
ban45
Contributor III

Hello,

What is the difference between 1.5kΩ ± 0.1% and 1.54kΩ ± 0.5%?

I couldn't understand why 0.1% was good by looking at the data sheet.
Could you tell me?

best regard

0 Kudos
Reply

592 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  "Using resistors with recommended tolerances ensures the ± 2% DDR_VREF tolerance
(per the DDR3 specification) is maintained when two DDR3 ICs plus the i.MX 6ULL are
drawing current on the resistor divider".

  You may look at the following general considerations:

https://www.maximintegrated.com/en/design/technical-documents/tutorials/7/719.html

In particular: Figure 4. This simple resistor-divider analogy represents a voltage reference
unloaded (A) and loaded (B).

 

Regards,
Yuri.

0 Kudos
Reply