Hi Team
I am using DDR test tool v3.0. I wanted to run the calibration test for Memory density - 1GB ( Micron - MT41K512M16VRN-107 IT:P) . The problem statement is I don't have script file to be loaded for this configuration. can any one provide proper script file for below configuration:
- 1GB memory density
- DDR operating freq is 400 MHz
- DRAM bus width is 16
Please provide the script file .inc for me to run the calibration.
Hi Yuri
Thank you very much for reply.
I already have this tool, but I need to load a script file for 1GB memory. to do calibration.
is my understanding right that script file is needed for different density memory ? current tool has script file of max 512MB only. can you please let me know on this issue
Hello,
Customers can use the following tool:
“i.MX6ULL_DDR3_Script_Aid”
https://community.nxp.com/docs/DOC-333791
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.