i.MX6ULL Clock out signal for AFE4490?!

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6ULL Clock out signal for AFE4490?!

361 Views
theevanvenugopa
Contributor II

Hey Team NXP!

I would like to provide clock pulse of 8MHz for one of my peripherals(AFE4490). I assigned the function to the below pin(P17). Is that Okay?

pastedImage_1.png

Labels (1)
0 Kudos
2 Replies

293 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Theevan,

You need to configure to run 8Mhz, configuration is described in sect. Miscellaneous Register 1 (PMU_MISC1n)

field LVDS1_CLK_SEL, i.MX6UL Reference Manual 

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

0 Kudos

293 Views
theevanvenugopa
Contributor II

@bio_ticfsl, I would like to check whether the pin P17 can be used for providing external clock of 8MHz to the External Peripheral(AFE4490)

Thank you.#clock output #External peripheral Clock #custom hardware

0 Kudos