硬件:i.MX6ull
软件:yocot_uboot_2016 + yocot_kernel_4.1.15
NXP的工程师们,我在使用i.MX6ULL的CAN的时候遇到了很奇怪的问题。现在将问题的描述如下:
首先,要使用CAN接口,高版本内核需要先适配其设备树。
<1>imx6ull-14x14-xxx.dts
&flexcan1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexcan1>;
xceiver-supply = <®_can_3v3>;
status = "okay";
};
&flexcan2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexcan2>;
xceiver-supply = <®_can_3v3>;
status = "okay";
};
pinctrl_flexcan1: flexcan1grp{
fsl,pins = <
MX6UL_PAD_UART3_RTS_B__FLEXCAN1_RX 0x1b020
MX6UL_PAD_UART3_CTS_B__FLEXCAN1_TX 0x1b020
>;
};
pinctrl_flexcan2: flexcan2grp{
fsl,pins = <
MX6UL_PAD_UART2_RTS_B__FLEXCAN2_RX 0x1b020
MX6UL_PAD_UART2_CTS_B__FLEXCAN2_TX 0x1b020
>;
};
<2>imx6ull.dtsi这个文件不用修改
flexcan1: can@02090000 {
compatible = "fsl,imx6ul-flexcan", "fsl,imx6q-flexcan";
reg = <0x02090000 0x4000>;
interrupts = <GIC_SPI 110 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_CAN1_IPG>,
<&clks IMX6UL_CLK_CAN1_SERIAL>;
clock-names = "ipg", "per";
stop-mode = <&gpr 0x10 1 0x10 17>;
status = "disabled";
};
flexcan2: can@02094000 {
compatible = "fsl,imx6ul-flexcan", "fsl,imx6q-flexcan";
reg = <0x02094000 0x4000>;
interrupts = <GIC_SPI 111 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_CAN2_IPG>,
<&clks IMX6UL_CLK_CAN2_SERIAL>;
clock-names = "ipg", "per";
stop-mode = <&gpr 0x10 2 0x10 18>;
status = "disabled";
};
<3>驱动程序为flexcan.c,此处无需任何改动
======================================
>>> 编译生成uboot.imx、zImage、dtb
>>> 烧写成功,系统启动 !!!
======================================
系统启动后,通过ifconfig -a查看can0、can1已经存在,只是没有启动
按照“i.MX_Linux_Reference_Manual”中的指导,执行以下命令:
ip link set can0 down
ip link set can0 up type can bitrate 500000
can1也是一样的操作,至此can0、can1 all becomes ready !!!
下面硬件连接can0与can1,HH相连,LL相连。执行以下命令:
candump can1 &
cansend can0 123#1122334455667788
问题来了,为什么can1口接收不到任何数据?我用示波器测量了cpu直接出来的pins,也没有任何波形。
尝试了各种角度,依旧没有找到问题的原因。
a.怀疑pin脚功能被定义错误,仔细检查了uboot和kernel中并没有出现复用其他功能的情况,读取寄存器的值也是正常的 0x20
b.尝试替换官方evk的zImage和dtb后,上述问题依然存在
c.can0发送,can1接收的过程中,ifconfig观察RX、TX的数据变化,遇到了不正常的现象
开始发送接收前:
开始后:
需要的话,附件为我的内核config文件和dts文件,请查阅。
请NXP的FAE or AE ,帮忙解决下这个问题,谢谢。
Any idea how to make following commands:
ip link set can0 down
ip link set can0 up type can bitrate 500000
ip link set can1 down
ip link set can1 up type can bitrate 500000
to be executed automatically on boot of device?
Tried to place it in 02_network init script but it throws me:
Cannot find device "can0"
Cannot find device "can0"
Cannot find device "can1"
Cannot find device "can1"
Hi jimmychan ,
我已经试过了将flexcan1和flexcan2的4个pin分别作为GPIO来操控,如下
MX6UL_PAD_UART3_RTS_B__FLEXCAN1_RX ===》 MX6UL_PAD_UART3_RTS_B__GPIO1_IO27
MX6UL_PAD_UART3_CTS_B__FLEXCAN1_TX ===》 MX6UL_PAD_UART3_CTS_B__GPIO1_IO26
MX6UL_PAD_UART2_RTS_B__FLEXCAN2_RX ===》 MX6UL_PAD_UART2_RTS_B__GPIO1_IO23
MX6UL_PAD_UART2_CTS_B__FLEXCAN2_TX ===》 MX6UL_PAD_UART2_CTS_B__GPIO1_IO22
分别输出高、输出低,来回切换,测得的电压均正常变化,所控制的led亮灭均正常。
L4.1.15是i.mx6ull官方SDK中推荐使用的版本,您的意思是让我再升级一下SDK吗?请问有哪个版本推荐的吗?
I don't see any problem on your setup.
You may double check the hardware pins are good connected.
Have you try to configure the CAN pins to GPIO? and then output 1 or 0 to see the pins are output proper.
L4.1.15 is an old BSP version. Have you try a newer version of BSP?