i.MX6UL un-powered pin stress

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6UL un-powered pin stress

Jump to solution
287 Views
kanoumamoru
Contributor III

Question about i.MX6UL concern with electric stress.

External I2C bus is always on. This bus is connected to i.MX6UL I2C pins (multiplex pin).

I2C voltage is keeping when i.MX6UL is completely power off status (all power off of i.MX6UL).

In this situation, Are there any electrical damage for i.MX6UL?

My customer feel nervous that i.MX6UL will lead to breakdown in this case.

If answer is yes, we should separate i.MX6's I2C bus when i.MX6UL is going to power off.

Best Regards,

kanou

Labels (1)
0 Kudos
1 Solution
93 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Kanou

you are right, external voltages should not be applied to processor

untill it fully powered up. This is described in sect.4.2.1 Power-up sequence

i.MX6UL Datasheet

NOTE
Need to ensure that there is no back voltage (leakage) from any supply on
the board towards the 3.3 V supply (for example, from the external
components that use both the 1.8 V and 3.3 V supplies).

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
94 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Kanou

you are right, external voltages should not be applied to processor

untill it fully powered up. This is described in sect.4.2.1 Power-up sequence

i.MX6UL Datasheet

NOTE
Need to ensure that there is no back voltage (leakage) from any supply on
the board towards the 3.3 V supply (for example, from the external
components that use both the 1.8 V and 3.3 V supplies).

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos