Hi,
Trying to get MQS working on a i.MX6UL project. I have the following in my board DTS:
&mqs {
clock-names = "mclk";
status = "okay";
};
When I boot up the system, I see the following kernel messages:
ERROR: could not get clock /soc/aips-bus@02000000/mqs:mclk(0) │
fsl-mqs 2000000.aips-bus:mqs: failed to get the clock: -2
So, looking for clues and ideas how to configure this. The ref manual has the following:
The user needs to program SAI1 to output 2-channel MSB-16bit active I2S signal, and
then to program the related IOMUXC_GPR2 bits.
Attached is a de-compiled version of my DTB, so you have a complete snapshot of my DT config.
Appreciate any pointers or an example of a platform that has this working that I could reference.
Thanks,
Cliff
Original Attachment has been moved to: x.dts.zip
Hi Cliff
mqs example can be found in imx6ul-14x14-ddr3-arm2-mqs.dts
linux-2.6-imx.git - Freescale i.MX Linux Tree
documentation: fsl,mqs.txt,imx-audio-mqs.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------