i.MX6UL fast-path function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL fast-path function

1,323 次查看
tangwang
Contributor I

Whether i.MX6UL can handle LAN/WAN configuration(via VLAN config) or not ? like what Ethernet switch did(routing package from LAN to WAN without consume CPU computing power) ? if no, what is the computing power need if we want to implement it(routing feature) by NXP CPU ? will this increase package latency ?

标签 (1)
0 项奖励
回复
2 回复数

1,203 次查看
tangwang
Contributor I

Hi Sir,

Do you have any example or source code for our reference?

0 项奖励
回复

1,203 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tang

I am afraid there is no hardware support for such capability and

cpu usage is needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 项奖励
回复