i.MX6UL WDOG_ANY port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL WDOG_ANY port

Jump to solution
940 Views
sugiyamatoshihi
Contributor V

Hi, 

I checked watch dog behavior by unit_test/wdt_driver_test.out.

Watch dog reset output WDOG1_WDOG_ANY on LCD_RESET ALT4 in i.MX6UL EVK.

I modified one thing, C738 was removed not to shut down DCDC_3V3, because customer don't want to power down the hole system.

At the first boot,  WDOG1_WDOG_ANY is high after Linux boot, then I entered wdog test command that is unit_test/wdt_driver_test.out 1 1 1 and system shut off and reboot.

After it reboot, WDOG1_WDOG_ANY doesn't become high. 

I confirmed that LCD_RESET pad set to ALT4  WDOG1_WDOG_ANY, but  pin level is low.

How can I set WDOG1_WDOG_ANY to high?

Best Regards,

Sugiyama

Labels (1)
1 Solution
860 Views
Yuri
NXP Employee
NXP Employee

Hello,

    The WDOG output pin will reset after POR, the internal WDOG reset does not affect it.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
860 Views
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thank you for reply.

I understood it need POR.

Best Regards,

Sugiyama

861 Views
Yuri
NXP Employee
NXP Employee

Hello,

    The WDOG output pin will reset after POR, the internal WDOG reset does not affect it.

Regards,

Yuri.

0 Kudos
Reply