i.MX6UL VHIGH SHORTED WITH SNVS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL VHIGH SHORTED WITH SNVS

691 Views
nachodiz
Contributor III

Dear all

For final design with I.MX6UL + PF3001A7 i want to short SNVS with VDDHIGH

I placed an external always ON LDO because PMIC SNVS provides only 1mA and the PMIC V33 LDO out is not always on (is part of secuence) and is not suitable to pullup the PMIC ON REC domain

I placed a 400 mA always ON LDO @ 3.3V for generating a ultra power SNVS AND VHIGH Voltage Source (+3.3V ALWAYS)

Its better to use a 3.0V LDO or can i go with 3.3V LDO?

Do i need any kind of Schotkky Diode?

NOTE: peripherials are powered from PMIC DCDC, 3.3VALWAYS ITS ONLY USED TO SUPPLY A SMALL PIC MCU AND SNVS AND VHIGH

kING rEGARDS

alw.png

0 Kudos
Reply
1 Reply

569 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nacho

>Its better to use a 3.0V LDO or can i go with 3.3V LDO?

all values are fine as both VDD_SNVS_IN and VDD_HIGH_IN

suitable according to Table 11. Operating Ranges

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply