Hi all
I have a question about MFGTool fail.
My customer want to boot from eMMC in i.MX6UL.
However, it stuck at "UTP Waiting for device to appear" message.
I tested following solution but it still have stuck at same message.
https://community.nxp.com/thread/316376
Do I need to set another configuration for Kernel ?
Here is a there environment.
Board: Custom board
OS: Linux L4.1.15
MFGTool: L4.1.15
If you need more information to advice, please ask me.
Ko-hey
Please refer this document regarding to booting i.MX6UL board from eMMC:
https://community.nxp.com/docs/DOC-331378
Of course you need to update the configuration accordingly to differences between custom board and EVK one.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi b36401
Thank you for reply but I can't open the link.
I get the message "Unauthorized".
Could you check again ?
Ko-hey