i.MX6UL USB OTG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL USB OTG

2,107件の閲覧回数
martinwerner
Contributor I

I have a question regarding the USB OTG interface on the IMX6UL. I am using the i.MX6UL in a custom Hardware Design and I am wondering if it is neccessary to set the ID Signal High or Low by external Components. I need a lot of Interfaces and Analog Inputs, so the muxed Pins ID, OC and PWR are blocked by other functions.

Is it possible to set these by Software?

Best regards

Martin

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,774件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

per usb specification ID signal should be high (or float) in Device mode,

low in Host. It is used by linux driver,  I am afraid it is not possible to set it by software

without additional modifications in linux sources.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,774件の閲覧回数
martinwerner
Contributor I

BTW: I want to use the i.MX6 as USB Host.

0 件の賞賛
返信