i.MX6UL: UART serial download disabled selection fuse.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL: UART serial download disabled selection fuse.

Jump to solution
1,046 Views
jean-christoph4
Contributor II

In the i.MX6UL RM, there is a description of a fuse named "UART serial download disabled selection" at location 0x470 (bit 4).

There is not a lot more description about this fuse. In particular, how different is it from the SDP_DIABLE fuse at location 0x460 (bit 17).

Could you provide an explanation on the relative use of these 2 fuses?

Thanks

JC

Labels (1)
Tags (2)
0 Kudos
1 Solution
944 Views
Yuri
NXP Employee
NXP Employee

Correct, if  SDP_DISABLE is set, no need to set "UART serial download disabled selection".

~Yuri.

View solution in original post

0 Kudos
3 Replies
944 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    "UART serial download disabled selection" relates to UART only.

SDP_DISABLE concerns both UART and USB.

Both fuses provide workarounds against the Vulnerability.

 

https://community.nxp.com/docs/DOC-334996 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
944 Views
jean-christoph4
Contributor II

So if I set SDP_DISABLE, I don't really need to set "UART serial download disabled selection" (event if it should not cause any trouble to also set "UART serial download disabled selection"), right?

Thanks.

JC

0 Kudos
945 Views
Yuri
NXP Employee
NXP Employee

Correct, if  SDP_DISABLE is set, no need to set "UART serial download disabled selection".

~Yuri.

0 Kudos