i.MX6UL UART DCE/DTE mode refers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL UART DCE/DTE mode refers

550 Views
amsol
Contributor I

Good day,

i.M6UL refers -  (based on variscite SOM  Yocto build )

I recently discovered, on completion and now production of my hardware platform,

 that I have interpreted UART DCE/DTE Modes incorrectly -

Unfortunately the correct doc-info only came forward once we went into production with you,

making me aware of the following issue -

In my design, as seen from the processor, the following h/w pad/pin config has been wired -

RXD < in

TXD > out

RTS > out

CTS < in

Testing on h/w platform (DCE mode) the serial comms work with h/w flow OFF

 When enabled, no comms, since in DCE mode RTS dir = in,  CTS dir = out.

 

In DTE mode, RTS dir out, CTS dir in, but TXD = in,  RXD = out.

  This also presents a problem, since now there will be no serial comms,

   since txd/rxd dir is reversed, with reference to my h/w wiring-

What I would like to know, are there any additional register-set configuration

 to allow my h/w config to work, iow, to allow my particular h/w configuration to work,

or is the only option to scrap the production units, (clearly the last option)

  or to modify  > swop RTS/CTS signals with jumpers in DCE mode,

   or to swop  TXD/RXD in DTE with jumpers.

Thank you for your advice on this matter.

Regards,

Gerhard Laubscher

Cape Town

South Africa

0 Kudos
Reply
1 Reply

501 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gerhard

unfortunately there are no any additional register-set configurations for

changing UART DTE/DCE functionality so one can consider using jumpers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply