i.MX6UL: SRK_REVOKE description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL: SRK_REVOKE description

Jump to solution
779 Views
jean-christoph4
Contributor II

In the i.MX6UL RM (and SRM) the SRK_REVOKE fuse is referenced.

But its exact location is never given.

We know it is 3 bits [2:0] long but we don't know where it is located.

Could you specify where this fuse is located in the i.MX6UL?

Thanks

JC

Labels (1)
Tags (2)
0 Kudos
1 Solution
720 Views
Yuri
NXP Employee
NXP Employee

Yes, 0x6F0.

~Yuri.

View solution in original post

0 Kudos
3 Replies
720 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    According to table in section 35.5 (OCOTP Memory Map/Register Definition)  

of i.MX 6UltraLite  Reference Manual, Rev. 2, 03/2017:

   fuse Bank 5 Word 7  is SRK Revoke.

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
720 Views
jean-christoph4
Contributor II

So if it was to be described in theTable 5-9 of chapter 5 (Fusemap) SRK_REVOKE would be at 0x6F0[2:0].

Is this correct?

Thanks.

JC

0 Kudos
721 Views
Yuri
NXP Employee
NXP Employee

Yes, 0x6F0.

~Yuri.

0 Kudos