In the i.MX6UL RM (and SRM) the SRK_REVOKE fuse is referenced.
But its exact location is never given.
We know it is 3 bits [2:0] long but we don't know where it is located.
Could you specify where this fuse is located in the i.MX6UL?
Thanks
JC
Solved! Go to Solution.
Hello,
According to table in section 35.5 (OCOTP Memory Map/Register Definition)
of i.MX 6UltraLite Reference Manual, Rev. 2, 03/2017:
fuse Bank 5 Word 7 is SRK Revoke.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
So if it was to be described in theTable 5-9 of chapter 5 (Fusemap) SRK_REVOKE would be at 0x6F0[2:0].
Is this correct?
Thanks.
JC
Yes, 0x6F0.
~Yuri.