i.MX6UL SPI DMA receive error occurr (first time only)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL SPI DMA receive error occurr (first time only)

1,400 Views
tomohisa_sakamo
Senior Contributor II

Dear support-team,

We found SPI DMA receive error occurr (first time only) by i.MX6ULL.
Condition:i.MX6ULEVK,L4.1.15_2.0.0/L4.1.15_1.2.0

We can look like similar cases(https://community.nxp.com/thread/339957 etc).
But we can not solve this problem.

If you have any workaround,Please inform us.

Best Regards,

Labels (1)
0 Kudos
Reply
4 Replies

1,180 Views
tomohisa_sakamo
Senior Contributor II

Hi Carlos,

We are sorry that our response was delayed.

Please refer below conditions.

Conditions>
===================================================================
Parameter at SPI transfer is as follows.

Bits per word: 16
Max speed Hz: 1660000
Tx data: 256 bytes of data

In order to transfer DMA, it is necessary to transfer data of 65 bytes or more.
===================================================================

Could you confirm it?

Best Regards,

0 Kudos
Reply

1,180 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi, you are mentioning the transfer values, but not extended details. Could you please be more specific like trying to reproduce the issue step by step?

Best regards!

/Carlos

0 Kudos
Reply

1,180 Views
tomohisa_sakamo
Senior Contributor II

Hi Carols,

We are sorry that our response was delayed.

We are sending detailed data using tickets, so please check that.

Best Regt Reards.

0 Kudos
Reply

1,180 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please specify the followed steps in order to reproduce the issue?

We will be waiting for your reply.

 

Best regards!

/Carlos

0 Kudos
Reply