i.MX6UL SNVS current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL SNVS current

724 Views
TammyTsai
Contributor III

Hi NXP team,

I would like to ask a question about the Battery Backup current.

The current of VDD_SNVS_IN of i.MX6UL will reach up to 500 uA.

Even if TAMPER PINs are not used, it will still be 205uA.

Using a CR2450 battery (about 550 mAh), such current consumption will run out of power in 2 months.

Products from other manufacturers have a maximum of around 20uA, or even less than 10uA.

image004.pngimage006.pngimage008.pngimage010.pngimage015.png

Does NXP have any improvement plans or other suggestions for battery backup?

 

Best Regards,

Tammy

Labels (1)
0 Kudos
Reply
3 Replies

677 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @TammyTsai,

I hope you are doing well.

Please refer to the latest i.MX 6UltraLite Power Consumption Measurement Application Note. The current consumption in the SNVS domain is 22uA as mentioned in Table 10. SNVS measurement results. Apart from this, no other data is available.SNVS.PNG

 I hope it helps!

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

565 Views
TammyTsai
Contributor III

Hi @riteshmpatel,

Thanks for your reply.

TammyTsai_0-1696569480888.png

How to address the BOOT_MODE requirement of step 2?

Could I switch BOOT_MODE by software?

Could you please described the method in detail?

 

Best Regards,

Tammy

0 Kudos
Reply

558 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @TammyTsai,

I request you to please raise a new ticket for the additional query.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply