i.MX6UL GPIO Pad Configuration & OpenOCD Signal Issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL GPIO Pad Configuration & OpenOCD Signal Issues

497件の閲覧回数
dev_imx
Contributor I

I am attempting to use an IMX6UL as a JTAG interface utilizing OpenOCD's native bitbang support for the IMX's GPIO.

I have successfully connected to the target at lower speeds such as 100KHz. However, to successfully perform flash functions, I need to set the adapter to speed to at least 500KHz, preferably closer to 1500KHz, and have not yet been able to connect to the target at these higher speeds. I have tried a host of GPIO Pad Control Configurations to optimize the signal output but have yet to find one that can properly handle these high speeds.

Therefore, I have the following two questions:

  1. What is the best possible GPIO pad configuration to reach these high speeds?
  2. Is it possible to toggle the GPIO registers using the IMX6UL at these higher speeds(500KHz,1500KHz,etc)?

 

タグ(2)
0 件の賞賛
返信
1 返信

467件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which pad are you using?

For example: You could check the pad control setting in the RM.

IOMUXC_SW_PAD_CTL_PAD_GPIO1_IO00

 

You could try to set the speed and the SRE of the PAD.

 

0 件の賞賛
返信