Hi community,
When run command to let system enter Deep-Sleep mode, I got the result: total current 39mA, voltage 5V.
The measurement and the official results, far from. Why?
Best Regards,
Steven
Solved! Go to Solution.
Could you please confirm the result is measured from the resitors?
Document Number: AN5170 i.MX 6UltraLite Power Consumption Measurement
Could you please confirm the result is measured from the resitors?
Document Number: AN5170 i.MX 6UltraLite Power Consumption Measurement
Hi Steven
please measure power consumption on 0.02 Ω resistors using
sect.3.7. Measuring points on the MX6UL EVK platform and sect.6.1. Deep-Sleep mode
AN5170 i.MX6 UltraLite Power Consumption
http://www.nxp.com/assets/documents/data/en/application-notes/AN5170.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------