i.MX6UL DDR3 Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL DDR3 Design

1,005 Views
ricardoferreira
Contributor II

Hi,

In the i.MX 6UltraLite Evaluation Kit design, the DDR3 the Address, command and control group are not routed in the same plane. I though these signals needed to be in the same plane. The aproach made in the evaluation board make the routing much easier but is it safe?
Is there any special rule I should follow to route some of these signals in different layers?

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

609 Views
woutersintecs
Contributor II

In general, keep things for the Address/Command/Control bus even, meaning the same length, same reference plane and the same amount of vias.

0 Kudos
Reply

609 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ricardo

this is common approach, described for example in micron app note

https://www.micron.com/~/media/documents/products/technical-note/dram/tn4614.pdf

allowing minimize crosstalk noise. More layout rules can be found in

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply