Hello,
Let me know for DDR3L interface of .MX6UL, does CPU supports the pin swapping features for data lines.With this feature we can connect any of the data line (D0:16) to any of the data lines. No one to one connection is required i.e. D0 to D0, D1 to D1 and so on.
This helps us for PCB layout.
Regards,
Surendra
Hi Surendra
please refer to sect.3.5.1 Swapping data lines
Hardware Development Guide for the i.MX 6UltraLite Applications Processor
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------