Hello, we are using the i.MX6UL platform and I need to observe the arm_root_clk on CCM_CLKO2 on the SD1_DATA2 pad as detailed in the RM. We are doing this because we need a visual representation of our operating frequency. My settings are as follows:
CCM Clock Output Source Register (CCM_CCOSR) (0x20C_4060h)
- set to value 0x018a0100
- this selects arm_root_clk for CLKO2 with divider of 5
SW_MUX_CTL_PAD_SD1_DATA3 SW MUX Control Register (IOMUXC_SW_MUX_CTL_PAD_SD1_DATA3) (0x20E_01D0h)
- set to value 0x00000006
- this selects ALT6 mode for CCM_CLKO2
SW_PAD_CTL_PAD_SD1_DATA3 SW PAD Control Register (IOMUXC_SW_PAD_CTL_PAD_SD1_DATA3) (0x20E_045Ch)
- set to value 0x0001F0D9
- this sets 200Mhz max pad freq
With these setting I am unable to see a clock on SD1_DATA2. If I change CCM_CCOSR to 0x010e0000 I will see the 24Mhz osc_clk correctly. I can also seem to see all other CLKO2 clocks - just not the one I need.
Is there something further I need to do to view the arm_clk_root clock?
Solved! Go to Solution.
Hi michaelschell
unfortunately i.MX6UL has not selection CLKO2_SEL= 01010 arm_clk_root,
it is reserved :
i.MX6UL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi michaelschell
unfortunately i.MX6UL has not selection CLKO2_SEL= 01010 arm_clk_root,
it is reserved :
i.MX6UL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks so much igor. Im clearly using the wrong version of the i.MX6UL reference manual. Mine does not show that value (01010) as reserved but instead specifies it for arm_clk_root. Ill move forward with this version of the RM. To your knowledge then, for the i.MX6UL, is there no way to export the arm clock (cpu clock rate) off chip?