i.MX6SX - Wake up from Stop mode with USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SX - Wake up from Stop mode with USB

2,070件の閲覧回数
davidjaouen
Contributor III

Hi,

I'm trying to wake up the i.MX6SX from stop mode when I plug in USB.

The USB is configured as a device and I want the i.MX6 to wake up when I plug it to a host.

Is there a way to do this with the i.MX6SX?

I tried to configure the USB PHY so a wake up IRQ triggers once activity is detected on DP/DM lines, but the SoC never wakes up when I plug the USB to a Host. Maybe I'm missing something in clocks and/or power configuration before entering stop mode. I didn't find any information on Stop mode exit in the USB PHY chapter in the i.MX6SX reference manual.

Regards,

David

ラベル(1)
タグ(2)
1 返信

1,800件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi David

please check sect.39.3.6 USB Wakeup Usage attached Linux Manual and

imx-test package, folder ../mxc_usb_test/doc     

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------