i.MX6SX UART clock during uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SX UART clock during uboot

ソリューションへジャンプ
1,934件の閲覧回数
torus1000
Contributor V

Hi,

I tested UART of i.MX6SX then I found UART clock switched from OSC to PLL3 during boot up of linux.

It caused error/unexpected data feeding on UART which assigned to Cortex-M4 in our case.


Why UART clock changed from OSC @uboot to PLL3 @linux?

Is there any way to supply PLL3 clock to UART from the beginning?

Can anyone help me?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,708件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi torus,

when Linux starts it takes all the hardware configurations from the device tree, so if the device tree has a different configurations from uboot it will change. Of you want to keep the same configuration you must edit the device tree. Here you will find UART node and you can set the clock here. As this is a quite extensive topic I can provide you with some useful links.

Definitive GPIO guide - Studio Kousagi Wiki 

Device Tree Tutorial (ARM) | Linux Kernel For Newbies 

Device Tree Made Easy 

https://events.linuxfoundation.org/sites/events/files/slides/petazzoni-device-tree-dummies.pdf 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,709件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi torus,

when Linux starts it takes all the hardware configurations from the device tree, so if the device tree has a different configurations from uboot it will change. Of you want to keep the same configuration you must edit the device tree. Here you will find UART node and you can set the clock here. As this is a quite extensive topic I can provide you with some useful links.

Definitive GPIO guide - Studio Kousagi Wiki 

Device Tree Tutorial (ARM) | Linux Kernel For Newbies 

Device Tree Made Easy 

https://events.linuxfoundation.org/sites/events/files/slides/petazzoni-device-tree-dummies.pdf 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,708件の閲覧回数
torus1000
Contributor V

Dear Carlos, @Carlos_Musich

Just in case, I would like to confirm about my guess that there is no particular reason to choose PLL3.

Is it correct?

BR

0 件の賞賛
返信