i.MX6SX IBIS for industrial chip.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SX IBIS for industrial chip.

Jump to solution
701 Views
satoshishimoda
Senior Contributor I


Hi community,

I have a question about i.MX6SX IBIS file.

I want to know which file (consumer or automotive) should I use for simulation with i.MX6SX industrial chip.

I found Which type IBIS model should I select using with industrial i.MX6DL ? , so I guess automotive file should be used for i.MX6SX also.

Is this right?

Best Regards,

Satoshi Shimoda

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
580 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
581 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply