i.MX6SL not booting and nothing on uart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SL not booting and nothing on uart

ソリューションへジャンプ
1,739件の閲覧回数
sagarus
Contributor I

I have a problem with booting up a imx6sl board. I have connected the USB to UART to my machine running Ubuntu at 115200 baud and when I apply power to the board I do not get any output from the UART. I also have the Android flash installed in SD2 slot, which I have tried both flashes and tried to create my own.

This is a band new board I just got, I have tried a imx50 and imx53, which both boot and display data on the UART port.

The Switches on the board match the silk screen any suggestions?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,522件の閲覧回数
sagarus
Contributor I

It turns out the evk I got did not have the processor solder to the board, I retuned the board and got one with a processor and now U-boot comes up :-)

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,522件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Which board is that? How did you build U-boot? FSL U-boot does support mx6sl_evk board that you could use as a reference.

0 件の賞賛
返信
1,523件の閲覧回数
sagarus
Contributor I

It turns out the evk I got did not have the processor solder to the board, I retuned the board and got one with a processor and now U-boot comes up :-)

0 件の賞賛
返信