i.MX6SL not booting and nothing on uart

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6SL not booting and nothing on uart

跳至解决方案
1,645 次查看
sagarus
Contributor I

I have a problem with booting up a imx6sl board. I have connected the USB to UART to my machine running Ubuntu at 115200 baud and when I apply power to the board I do not get any output from the UART. I also have the Android flash installed in SD2 slot, which I have tried both flashes and tried to create my own.

This is a band new board I just got, I have tried a imx50 and imx53, which both boot and display data on the UART port.

The Switches on the board match the silk screen any suggestions?

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,428 次查看
sagarus
Contributor I

It turns out the evk I got did not have the processor solder to the board, I retuned the board and got one with a processor and now U-boot comes up :-)

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,428 次查看
fabio_estevam
NXP Employee
NXP Employee

Which board is that? How did you build U-boot? FSL U-boot does support mx6sl_evk board that you could use as a reference.

0 项奖励
回复
1,429 次查看
sagarus
Contributor I

It turns out the evk I got did not have the processor solder to the board, I retuned the board and got one with a processor and now U-boot comes up :-)

0 项奖励
回复