i.MX6SL is not booting up when using MCIMX6L2EVN10AB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6SL is not booting up when using MCIMX6L2EVN10AB

7,272 次查看
daeyonglee
Contributor I

Hi. All.

 

Our board based on i.MX6SL EVK board and using MCIMX6L8DVN10AB.

(platform : imx-3.10.17-1.0.0_ga, Boot CFG: eMMC using uSDHC2, LPDDR2, without LCD)

 

But when changed only chip from MCIMX6L8DVN10AB to MCIMX6L2EVN10AB, our board is not booting up.

(Also download firmware is not working by mfgtool)

(S/W Side: When power on, i can't see console messages for boot up.)

(H/W Side: DDR stress test is working but board is still booting up.)

 

I ask your opinion what tasks need to know in order to solve this problem.

 

Thank you for your support.

Original Attachment has been moved to: mfgtool2-imx6sl-es2-sdcard-emmc.vbs.zip

Original Attachment has been moved to: player.ini.zip

Original Attachment has been moved to: ddr_calibration_20160616-20'15'54.log.zip

Original Attachment has been moved to: imximage.cfg.zip

Original Attachment has been moved to: ucl2.xml.zip

标签 (1)
0 项奖励
回复
10 回复数

6,967 次查看
daeyonglee
Contributor I

Hi igor.

Sure. you're right.

So i have built image for each of boards.

Board 8D: core-image-base

Board 2E: fsl-image-manufacturing

Case Board 8D, put u-boot.imx,uImage and uImage-imx6sl-evk-ldo.dtb by "fsl-image-manufacturing", no matter operates

Anyway... my point that "Board 2E" is not starting download  process (images by "fsl-image-manufacturing").

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
daeyonglee
Contributor I

Hi igor.

Surrmary:

I have two boards.

Board 8D: with MCIMX6L8DVN10AB

Board 2E: with MCIMX6L2EVN10AB

The board 8D is booting ok with u-boot.imx( with imximage.cfg-included above calibration data-)

In other words, i have tried to download firmware to two boards with same u-boot.imx,uImage and uImage-imx6sl-evk-ldo.dtb .

(boot and uImage are built by fsl-image-manufacturing)

Board 8D is download firmware ok and booting ok.

But Board 2E is not starting download process.

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DaeYong

this is expected behaviour as for two different

boards two different images may be needed

Best regards

igor

0 项奖励
回复

6,967 次查看
daeyonglee
Contributor I

Hi igor

I guess that maybe issue for mfgtool have another issue.

Case normal download firmware)

After Starting kernel... , right now show blew messages...

Booting Linux on physical CPU 0x0

Linux version 3.10.17-1.0.0_ga+g232293e (korea@korea-H67M-D2-B3-2) (gcc version 4.8.1 (GCC) ) #2 SMP PREEMPT Fri Oct 10 12:13:04 KST 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 SoloLite (Device Tree), model: Freescale i.MX6 SoloLite EVK Board

cma: CMA: reserved 320 MiB at 8c000000

Memory policy: ECC disabled, Data cache writealloc

..................................................................................................................................................................................

But issue case)

After Starting kernel... , i can't see anything messages "Booting Linux on physical CPU 0x0"

(What is mean "Booting Linux on physical CPU 0x0"?)

Please let me know your opinons.

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DaeYong

is board booting OK with the same imximage.cfg,

but running bare linux ?

Best regards

igor

0 项奖励
回复

6,967 次查看
daeyonglee
Contributor I

Hi igor

Note that i have changed two points in the imximage.cfg.

MPRDDLCTL PHY0 (0x021b0848) = 0x40404448

MPWRDLCTL PHY0 (0x021b0850) = 0x4040342E

But mfgtool still did not produce any more progress after "Starting kernel ...."

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
daeyonglee
Contributor I

Hi igor

You mean that should i changed to DCD in the imximage.cfg?

Unfortunately, i didn't know how to change DCD.

So I did not make changes yet.

I have attached stress test log file and imximage.cfg.

If possible, please let me know more informations.

Thank you for your support.

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DaeYongLEE

MCIMX6L2EVN10AB has not gpu,epdc so please rebuild linux image

without these peripherals, check sect.13.1.1.6 Menu Configuration Options

attached Linux Manual. Note, for new processor part ddr test should be run and

new calibration settings provided in uboot ".cfg file.

Regarding mfg tools, it is necessary to rebuild firmware, removing from

image gpu,epdc, as shown in attached Yocto Guide Table 1. Freescale Yocto Project

images, "fsl-image-manufacturing".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,967 次查看
daeyonglee
Contributor I

Hi igor.

Thank you for your quick response.

I have build a image.

(the build image is "fsl-image-manufacturing-imx6slevk.ext3")

I have still problem for download firmeware.

When start download firmware, console message show last message "Starting kernel" and then don't processing next operation.

(Please note that below image)

mfgtool failed.PNG

The previous mfgtool using mfgtool2-imx6sl-es2-sdcard-emmc.vbs

I have read manual but i don't still know how to set mfgtool for "fsl-image-manufacturing-imx6slevk.ext3".

Please could you provide the relevant files or description?

Thank you for your support.

Best regards

DaeYong

0 项奖励
回复

6,967 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DaeYong

when built "fsl-image-manufacturing"

had you run ddr test and entered new calibration settings in uboot ".cfg file ?

~igor

0 项奖励
回复