i.MX6SL USB signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL USB signals

1,109 Views
dustinduong
Contributor I

We are having an issue with the USB port on the
IMX6SL.  The voltage swing of the USB D- & D+ are not meeting spec as
you can see in the Eye Diagram of the attachment.  Is there someone at
NXP/Freescale that can help me here?  These signal come directly from the
processor.  We only use USB Device mode only.

Labels (1)
0 Kudos
8 Replies

836 Views
karina_valencia
NXP Apps Support
NXP Apps Support

igorpadykov‌ can you help to continue with the follow up?

0 Kudos

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dustin

for tweaking of usb phy parameters one can follow

AN4589 Configuring USB on i.MX 6 Series Processors

http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf

Also recommended to check layout as described in sect.

3.11 USB recommendations i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

836 Views
dustinduong
Contributor I

Hi,

I have tried different combination on the USBPHYx_TXn register that contains the TXCAL45DP, TXCAL45DN and D_CAL to see if the DP and DN signal would increase to 3Volts with any luck.  According to the 53.2.6 section, changing these bit should have some effect on the output signal, we did not see any change of signal level.  Can you please explain why?

I have run print jobs from a standard PC computer and hooking up scope probes to the DN and DP signals.  The signals only swing from 0 to 2.68V.  Our system is in a device mode running FS (12Mhz).  We laid out the board trace for 90 ohm.   Also we have tried changing the value and we see no change in the output voltage.   Please help , we trying to launch the product.   Let us know if you need anything else.   Thanks.

0 Kudos

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dustin

could you check processor VDD_USB_CAP (should be 3.0V),

p.6 i.MX6SL EVK schematic spf-27452 and check p.9 USB section

Schematics (2)
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 1)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Voltage can be changed using PMU_REG_3P0 register. How many boards have this issue,

also could this be reproducable on i.MX6SL EVK, are signals ok in USB Host mode?

Please note that eye diagram is applicable to device which is be capable of sending the

Test_Packet pattern, that it should be in Host mode (just for reference attached usb\test\usb0_host_testmodes_test.c

with description in pdf document sect.34.9 Testing the host mode).

High Speed Eye 

Best regards
igor

0 Kudos

836 Views
dustinduong
Contributor I

Hi Igor,

The customer measured the VDD_USB_CAP and the voltage only gets to 2.58V. How do we get that voltage to 3V?

Dustin

0 Kudos

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dustin

seems processor is damaged or there are some board

layout errors (for example shortcircuits or broken traces).

Best regards
igor

0 Kudos

836 Views
dustinduong
Contributor I

Hi Igor,

The customer wants to know how to change the register PMU_REG_3P0 as you recommended earlier to get them up to 3V. Thanks.

Dustin

0 Kudos

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dustin

 

field OUTPUT_TRG register PMU_REG_3P0

sect. 36.7.2 Regulator 3P0 Register (PMU_REG_3P0)
there is no need to change it as it is set correctly, using nxp bsps from
0 Kudos