i.MX6SL HSIC connection when unused.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL HSIC connection when unused.

Jump to solution
1,317 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SL USB HSIC.

I want to know how connect the USB HSIC pads of i.MX6SL (HSIC_DAT an HSIC_STROBE) when USB HSIC is unused.

My understanding is as below, is this correct?

In boot sequence:

The out of reset condition of HSIC_xxx pads are input, but there is 100k ohm internal pull-down.

So it is no problem even if these pads are floating.

After boot:

HSIC_xxx pads can be used for GPIO, so it is no problem even if these pads are floating by set the pads to GPIO output pins.

Best Regards,

Satoshi Shimoda

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,187 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right: when HSIC is unused, no problem leave these pads floating

and they can be used for GPIO.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,188 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right: when HSIC is unused, no problem leave these pads floating

and they can be used for GPIO.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply