i.MX6SL BOOT_CFG2[7:6] setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL BOOT_CFG2[7:6] setting

Jump to solution
792 Views
torus1000
Contributor V


Hi,

i.MX6SL reference manual described different setting as attached.

Could anyone help me to clarify which one is correct?

Thanks.

Boot_config2_7-6a.png

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
687 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6 SL EIM does not support 16-bit Non Multiplexed Address/Data Mode with

data bus located on high data bytes. Please look at Table 36 (EIM Internal Module Multiplexing)
of i.MX6 SL Datasheet.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
688 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6 SL EIM does not support 16-bit Non Multiplexed Address/Data Mode with

data bus located on high data bytes. Please look at Table 36 (EIM Internal Module Multiplexing)
of i.MX6 SL Datasheet.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply