i.MX6SDL VPU cannot decode jpeg file with unit_test when the jpeg size is 1024 byte.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL VPU cannot decode jpeg file with unit_test when the jpeg size is 1024 byte.

Jump to solution
3,117 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL vpu decoding.

When decode a 1024 byte jpeg file with vpudec for gstreamer, vpu can decode it correctly.

On the other hand, when decode a 1024 byte jpeg file with unit_test in L3.0.35_4.1.0, vpu cannot decode it and the output size will be "0".

In this case, vpudec is not used and libvpu in imx-vpu is used.

So we guess imx-vpu is the root cause of this issue.

Then, would you let me know how to resolve this issue when use libvpu?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
2,609 Views
gfine
NXP Employee
NXP Employee

Hi Satochi,

Attached is a patch file.  You can either apply the patch or use the binary attached.

Please let me know the result.

Cheers,

Glen

View solution in original post

0 Kudos
Reply
7 Replies
2,609 Views
satoshishimoda
Senior Contributor I

Hi community,

I got additional information.

This issue occurs with the following condition.

=====

Format = YCC420

Some file can be decoded, it depends on body size excluding header part.

If add 1 byte to the file that this issue occurs and it will be 1025 byte, decode was succeed.

=====

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
2,609 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi again Satoshi,

Can you provide the steps to reproduce the problem?

Best Regards,

Alejandro

0 Kudos
Reply
2,609 Views
satoshishimoda
Senior Contributor I

Hi Alejandro,

I have tried sending the jpeg file, have you not yet received it?

If you have not received it, please tell me how to send the file as secret.

For your additional information, sometimes decoding was failed even if the size was 1025 bytes or Y42B format 1024 bytes image.

So would you investigate the condition when this problem occurs?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
2,610 Views
gfine
NXP Employee
NXP Employee

Hi Satochi,

Attached is a patch file.  You can either apply the patch or use the binary attached.

Please let me know the result.

Cheers,

Glen

0 Kudos
Reply
2,609 Views
yanfengliu
Contributor III

Glen,

Will this issue cause partial decoding of JPG input as Corrupted MJPG decoding result with FSL 3.10.17 BSP on i.MX6Q VPU?

Does this issue exist in FSL 3.10.17 release as well? If so, does the patch above patch apply as well?

Regards,

yf

0 Kudos
Reply
2,609 Views
gfine
NXP Employee
NXP Employee

Hi Yanfeng,

I am not sure.  The patch was for 3.0.35 and should be in newer versions. I'll double check if it was included but from the description of the thread you referenced. I think  that is more an mpeg problem than JPEG.

Can you provide a testcase to replicate the error?

Cheers,

Glen

0 Kudos
Reply
2,609 Views
satoshishimoda
Senior Contributor I

Dear Alejanro,

Sorry for delay.

I got the command to reproduce the problem.

./mxc_vpu_test.out -D "-i dump_copy.jpeg -o dump_copy_out.raw -f 7 -c 1"

And I will send you the jpeg file by message to use the above command.

Sorry, I cannot upload this jpg file here because this file was made by our partner, and I have not allowed to upload it to public space.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply