Hi community,
Our partner have a question about i.MX6SDL operating range.
Please see Table 9 in IMX6SDLCEC Rev.3.
LDO Output Set Point (VDD_ARM_CAP) when LDO enabled mode is same as VDD_ARM_IN(min) at operation up to 792MHz and up to 396MHz.
However, LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.
These are not same value.
We guess LDO Output Set Point = 1.225V @ up to 996MHz when LDO enabled is misprint, and correct value is 1.250V.
Is this correct?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
I received confirmation, that the Datasheet (Table 9 in IMX6SDLCEC Rev.3.) is correct
regarding LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I received confirmation, that the Datasheet (Table 9 in IMX6SDLCEC Rev.3.) is correct
regarding LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------