i.MX6SDL VDD_ARM_CAP LDO output set point @ 996MHz.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL VDD_ARM_CAP LDO output set point @ 996MHz.

ソリューションへジャンプ
874件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6SDL operating range.

Please see Table 9 in IMX6SDLCEC Rev.3.

LDO Output Set Point (VDD_ARM_CAP) when LDO enabled mode is same as VDD_ARM_IN(min) at operation up to 792MHz and up to 396MHz.

However, LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.

These are not same value.

We guess LDO Output Set Point = 1.225V @ up to 996MHz when LDO enabled is misprint, and correct value is 1.250V.

Is this correct?

Best Regards,

Satoshi Shimoda

ラベル(2)
0 件の賞賛
返信
1 解決策
660件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I received confirmation, that the Datasheet (Table 9 in IMX6SDLCEC Rev.3.) is correct
regarding LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
661件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I received confirmation, that the Datasheet (Table 9 in IMX6SDLCEC Rev.3.) is correct
regarding LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信