i.MX6SDL GC880 performance.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL GC880 performance.

Jump to solution
4,294 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL GPU performance.

I want to know the performance of GC880 in i.MX6SDL, but I did not find the following performances.

Pixel Rate (MPixel/sec)

Triangle Rate (M tri/sec)

Vertext Rate (M vtx/sec)

Shader GFLOPS

So would you let me kwno the performances?

Best Regards,

Satoshi Shimoda

Labels (3)
0 Kudos
Reply
1 Solution
2,737 Views
art
NXP Employee
NXP Employee

The available performance data for the Vivante GC880 3D graphics core are as follows.

Pixel rate is 266Mpix/s.

Triangle rate is 35Mtri/s.

Vertex rate is about 100Mvtx/s.

Shader GFLOPS rate is 3.2.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,738 Views
art
NXP Employee
NXP Employee

The available performance data for the Vivante GC880 3D graphics core are as follows.

Pixel rate is 266Mpix/s.

Triangle rate is 35Mtri/s.

Vertex rate is about 100Mvtx/s.

Shader GFLOPS rate is 3.2.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply