Hi community,
Our partner have a question about i.MX6SDL.
Actually, their board did not boot correctly from SD or NAND at u-boot when enabled HABv4 and using i.MX6S rev. 1.2.
The success rate to boot correctly is about 5%.
When using i.MX6S rev.1.1, this issue was not occurred even though HABv4 is enabled.
Do you know why boot with rev. 1.2 chip fails?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hello Satoshi San,
This is due to a change in the HAB API offset in the boot ROM. From REV 1.1 to REV 1.2. Unfortunately I do not have further details that I can exchange for you in the public community . Please enter an SR or contact your local Freescale FAE or Sales.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Satoshi San,
This is due to a change in the HAB API offset in the boot ROM. From REV 1.1 to REV 1.2. Unfortunately I do not have further details that I can exchange for you in the public community . Please enter an SR or contact your local Freescale FAE or Sales.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------