Hello,
According to our i.MX6S RM, it says i.MX6S can support SDXC as like below.
Up to 832 Mbps of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode
But, I wonder if our BSP can support SDXC as well and there is no problem to support over 1TB capacity as well. According to SDXC spec, it seems to support up to 2TByte but I am not sure if our BSP or file system can have limiation to do it.
Best regards,
Paul
Hello Paul,
Yes, the i.MX6 supports SDXC, as well as the BSP supports it.