i.MX6S SDXC support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S SDXC support

1,516 Views
Paul_Kang
NXP Employee
NXP Employee

Hello,

According to our i.MX6S RM, it says i.MX6S can support SDXC as like below.

Up to 832 Mbps of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode

But, I wonder if our BSP can support SDXC as well and there is no problem to support over 1TB capacity as well. According to SDXC spec, it seems to support up to 2TByte but I am not sure if our BSP or file system can have limiation to do it.

Best regards,

Paul

Tags (2)
1 Reply

1,260 Views
SergioSolis
NXP Employee
NXP Employee

Hello Paul,

Yes, the i.MX6 supports SDXC, as well as the BSP supports it.

0 Kudos
Reply