i.MX6S EIM synchronous access timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S EIM synchronous access timing

Jump to solution
587 Views
torus1000
Contributor V

Hi,

I am just curious about blank of IMX6SDLCEC datasheet as following.

imx6sdlcec_p52.png

Why setup/hold timing(WE18-21) didn't specify in case of BCD=2 or 3?
(Are those same as BCD=1?) 

Can anyone help me?

Thanks.

         Note: BCD=Burst Clock Divisor

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
511 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

you are right, those same as BCD=1, just for reference

one can check i.MX6DQ Datasheet where similar table is a bit clear.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
512 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

you are right, those same as BCD=1, just for reference

one can check i.MX6DQ Datasheet where similar table is a bit clear.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply