i.MX6Quad imx-viv-gpu 6.2.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Quad imx-viv-gpu 6.2.3

3,210件の閲覧回数
simobrazz
Contributor II

Hello,

I have some problems with the driver imx-viv-gpu 6.2.2p0 and GPU Vivante GC2000. In particular, the driver does not supports large OpenCL kernels (it always gave me out-of-resources error -5 and I'm using Debian OS).

The problem seems related to the actual driver version (as stated in this link), and could be solved with the 6.2.3 update.

Any update on the new version?

Best regards

タグ(3)
7 返答(返信)

2,303件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

try to use the newer yocto version, like 4.9.11, which includes the new driver version, pls try to use it

0 件の賞賛
返信

2,303件の閲覧回数
simobrazz
Contributor II

Where I can find it?

0 件の賞賛
返信

2,303件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

try to download it from the link as below:

i.MX 6Quad SABRE Development Board|NXP 

0 件の賞賛
返信

2,303件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

I don't have the full view on this topic at the moment, but I think that there is no 6.2.3 release for the i.MX6. In the 4.9.11 BSB release I can see the 6.2.2.

For the 4.9.51 based BSP platform releases for i.MX8 we have included version 6.2.4, but as this is a different GPU I'm not perfectly sure if it can be applied. I will check for the update plan for the i.MX6 platforms.

0 件の賞賛
返信

2,303件の閲覧回数
simobrazz
Contributor II

Any update on the 6.2.3 release?

0 件の賞賛
返信

2,303件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

Yes, I sorted it out.

  • 4.9.11ga release for the i.MX6 and i.MX7 devices includes 6.2.2, no gpu update one this
  • 4.9.51alpha for the i.MX8 devices included 6.2.3
  • 4.9.51ga for the i.MX8 devices includes 6.2.4

For a Vivante update on the i.MX6/7 devices on 6.2.4 (or later) we need to wait for a new BSP release.

You could use the latest driver 6.2.4 from an i.MX8M build on your own risk, the Vivante drivers are backwards compatible.

Regards,

Bernhard.

2,303件の閲覧回数
bernhardfink
NXP Employee
NXP Employee
0 件の賞賛
返信