i.MX6Qsabresd Board and Murata 1MW WiFi/BT connection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Qsabresd Board and Murata 1MW WiFi/BT connection problem

1,621件の閲覧回数
zh_y
Contributor II

I connected the two boards to page 28 of themurata_quick_start_guide_linux.pdf manual.At the same time, I built the new mirror file as described in the following post in the community https://community.nxp.com/thread/496328.

1) According to the above connection I will wfi test pass without problem,but I don't know how bluetooth should be connected to the board in the hardware part.According to table 10 on page 49 of the manual, it is indicated that I should connect GPIO2 and UART5. Where should the specific terminals be connected.

捕获.PNG

2) The above verification was done on the i.MX6Qsabresd Board.How to extract the patched Murata 1MW WiFi/BT kernel source code from yocto.

タグ(3)
0 件の賞賛
2 返答(返信)

1,464件の閲覧回数
romitchatterjee
Contributor V

Hi,

You will need to connect the Flat Flex Cable that came with the uSD-M.2 adapter. Check this post: https://community.murata.com/s/feed/0D55F000098u6o6SAA , which discusses how to connect the FFC.

In case you need clarifications or have further questions, feel free to contact Murata at their technical support forum: https://community.murata.com/ .

Best regards

 

0 件の賞賛

1,518件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I suggest that you enter your question in the Murata Technical Support, they can help you, with your inquiry since the module was directly made for the i.MX6 platform

Support | Murata Manufacturing Co., Ltd. 

0 件の賞賛